text.skipToContent text.skipToNavigation
Stimați parteneri, În data de 24.01.2025 o să fie Sărbătoare Națională în România, motiv pentru care comenzile dvs. înregistrate în 23.01.2025 se vor livra în data de 28.01.2025 iar cele inregistrate in 24.01.2025 se vor livra in 29.01.2025!
Semicon & Medical

Always the right fasteners within reach

Are you active in the Semicon & Medical industry (semiconductor and medical industry)? Then you have to deal with high-quality requirements and a strict project-based approach. As an indispensable link in a production process, you should not think about employees selecting the wrong fasteners. Fabory supports you during the run-up to a project, the project duration, and the aftercare phase (service & repair). With Fabory Logic's logistics solutions, you are assured of optimal fastener availability and your Total Cost of Ownership (TCO) remains as low as possible.

Fabory supports the Semicon & Medical sector with, among other things:

  • Production, construction, and overhaul of CT scan systems, MR imaging systems, and various other medical peripherals
  • Production of lithographic systems for making microchips
Medical
© ASML

Clean Room

Your production or assembly process determines the degree of technical cleanliness that applies to the fasteners and tools to be used. Together with our cleaning partners, we ensure that contaminants are removed from products and that they can be used in your application without risk of contamination. The cleaning processes focus on these types of pollution:

  • Residues from the production process such as burrs and chips
  • Residues from the production environment such as dust, fibers, and sand
  • Stains from process residues, corrosion inhibitors, or fingerprints

The degree of cleanliness required determines to what extent the above contamination may be present and which verification methods must be used to prove this. For some applications a check with (UV) light is sufficient and for other applications, a residual gas analysis (RGA) may be required.

In addition, it is important to consider not only the cleanliness requirements but also other metallurgical or tribological properties of the products. Sometimes other precautions are necessary. For example, it may be necessary to apply an EPK (electrolytic polishing & kolsterizing) treatment to guarantee the performance of the product in ultra-clean conditions.

Are you looking for a cleaning process like the one above or do you have a different set of requirements? Please do not hesitate to contact us to discuss the possibilities.

Fabory Logic solutions such as RFID and Weight Scale Cabinet can also be implemented in your cleanroom environment. This way you always have all the necessary items within reach.

Most ordered fasteners

Which fasteners do we see most often on the order lists of customers from this industry? These are the ten fasteners below:

Related products

At Fabory, we are not only specialists in fasteners. Related products are also part of our offer. Think of adhesives, sealants, lubricants, hand and power tools, safety equipment and clean room products. Delivering intelligent C-parts management is becoming increasingly important. Close cooperation with customers and suppliers results in a tailor-made range of products, services and expertise. Fabory experts advise you on optimal user-friendliness and reliable performance. Feel free to ask us your question about specific fastening solutions or the use of related products.

View our full range at Fabory.com

Semicon brands

This is why the Semicon & Medical sector chooses Fabory:

✓ Fast and flexible delivery of all types of fasteners that meet the specified specifications

✓ More than 150,000 different fasteners available from stock

✓ Based on your expected use, we deliver the cleanroom fasteners you require at the right time

✓ Fasteners are fully batch traceable thanks to the ISO9001 quality management system

✓ Quality control in Fabory's A2LA accredited laboratory

✓ Services such as Vendor Managed Inventory (VMI) on site and digital integrations such as MyFabory increase your ease of ordering.

Creating Peace of Mind

At Fabory, you can choose from over 150,000 fasteners. They come in any desired design, size and material type. Such an extensive range requires efficient stock management that you can rely on. Smart logistics solutions that provide insight into consumption help with this. With the use of both the RFID solution and the Weight Scale Cabinet you get access to your own VMI monitor in MyFabory. This provides insight into historical consumption of the stock and our performance. The combination of offering solutions and providing insight is unique.

In addition to these solutions, the Fabory experts provide advice, calculations and tests. They help to realise secure connections. This creates Peace of Mind, so that you and your employees can continue to focus on the core tasks.

Contact us to discuss the possibilities.

Medical

Punctele noastre tari

Gama de produse

Fabory este alegerea potrivită pentru toate nevoile dvs. de fixare. Portofoliul nostru de produse conține o gamă largă de elemente de fixare standard și soluții de fixare specifice pentru diverse aplicații precum si C-parts.

Fabory Logic

Fabory Logic va pune la dispozitie o gama completa de servicii lde gestionare a stocurilor printre care RFID, Optical-Eye, Cântare și Merchandiser

Inginerie si controlul calitatii

Fabory este construit pe calitate și fiabilitate. Managementul calității este în centrul operațiunii noastre. Inginerii noștri sunt disponibili pentru a vă sprijini în asigurarea alegerii corecte a elementelor de fixare.

Nu închideți această pagină. Acest mesaj va dispărea când pagina este complet încărcată.