text.skipToContent text.skipToNavigation
Header Food&Dairy

Les éléments de fixation en acier inoxydable qui vous conviennent ! 

Vous êtes un acteur dans la fabrication de machines pour l'industrie alimentaire ? Dans ce cas, il y a de fortes chances que vous disposiez de tôles, de profilés et d'éléments de fixation standard en acier inoxydable dans vos stocks. Sans les fixations suffisantes, aucune machine ne sera construite. Pourquoi tant d'entreprises font-elles confiance à l'acier inoxydable pour construire leurs machines ? Les clients nous donnent ces raisons :

  • La résistance du matériau
  • La résistance à la corrosion
  • La facilité de nettoyage
  • Hygiène et sécurité alimentaire
  • Durable et nécessite peu d'entretien
Food&Dairy

Most Commonly Used Fasteners in the Food Industry

Which fasteners do we see the most on the order lists of customers from the food industry?

The Fabory range includes more than 30,000 stainless steel fasteners, which you can order from stock on Fabory.com. Can't find the product you are looking for in the overview? Let us know because we will deliver it to you. In addition, we design and manufacture the product ourselves if it does not already exist.
 

Discover our range of stainless steel

Lubrinox: Pre-lubricated Bolts, Screws, and Nuts

Fabory has developed a new line of fasteners known as Lubrinox bolts, nuts, and screws. When using stainless steel fasteners, it is common for the inner and outer threads to seize together, making it difficult to loosen them. While applying a paste can prevent this issue, it requires additional time, and the workpieces and hands must be cleaned afterwards. Lubrinox has been specifically designed for the food industry to provide long-lasting lubrication in connections.

Below are the key advantages of Lubrinox:

  • Prevents galling of stainless steel bolt connections
  • Approved for use in the food industry
  • Pre-applied at Fabory, saving an average of 25 seconds per connection
  • Available in nuts as well
  • Maintains the stainless steel appearance of articles
  • Works effectively in combination with Loctite
  • Eliminates the issue of dirty hands from manual lubrication

Manufacturer of Coolers and Dryers

Geelen Counterflow, a design and production company based in Haelen, is one of the first to test Lubrinox. The lubricated fasteners are incorporated into coolers and dryers specially designed for the food industry. Geelen Counterflow ships several units of these coolers and dryers weekly to locations worldwide.

Due to the extensive use of stainless steel fasteners, the company sought a cost-effective alternative to traditional lubrication methods. René Derckx, the technical purchaser at Geelen Counterflow, stated, “We were curious whether the solution developed by Fabory would meet our needs. The primary requirement was to prevent threads from getting stuck. We wanted to avoid having to cut or drill out a screw.

Another coating that employees frequently use is significantly thicker. However, the Lubrinox fasteners do not require such a substantial layer. “A thick layer makes it difficult to drive screws by hand, causing them to become overly greasy. If you need to exert force, your fingers tend to slip over the hex. That doesn’t happen with Lubrinox. The feedback from the shop floor during this test has been positive,” he added.

Lubrinox
Stainless steel fasteners go into the Counterflow Cooler Plus
Captive screws & bolts

Captive Screws and Bolts

Finding a screw or bolt in food is something no one wants to encounter. However, securing fasteners in panels and doors that open and close frequently can be difficult. The Fabory range includes captive screws and bolts that feature a space-saving clip. This innovative locking clip eliminates the need for a locknut behind the panel. Additionally, these screws have a reduced shank, so you no longer need to tap threads into the panel holes. This solution was developed in collaboration with a customer who inspired the idea. We would happily work with you if your application requires a specific range extension. Please get in touch with us.

Hygienic Bolts and Nuts

For a food producer, periodic cleaning and disinfection of machines is essential. Washdown machines require fasteners with specific design features, such as smooth surfaces and minimal voids. We have developed the Fabory Premium Stainless Hygienic fasteners (FPS-H), which feature a smooth, polished surface and rubber sealing rings, to meet these needs.

Personalised Advice for Your Fastening Challenges

Our application engineers provide tailored solutions and advice on various fastening issues, including FDA regulations, hygiene, machinery safety, and corrosion resistance. Our close cooperation with standardisation institutes and technical committees ensures we have high technical knowledge and reliable information and service!

Optimising Processes Together

Fasteners may be a conservative product category, but we at Fabory are committed to continuous innovation. The food industry has trusted Fabory for years to supply stainless steel fasteners because:

  • Our fasteners are designed to enhance efficiency and comply with industry regulations.
  • Smart logistics solutions optimise fastener stock management and reduce the Total Cost of Ownership (TCO), leading to greater flexibility and cost control within your organisation.
  • Our Peace of Mind solutions ensure that production operations run smoothly.

Creating Peace of Mind

Fabory offers an extensive selection of over 120,000 fasteners in various designs, sizes, and materials. Managing such a large inventory requires reliable systems. Our smart logistics solutions provide insights into consumption patterns, significantly assisting inventory management. With our RFID solution and Weight Scale Cabinet, you can access your Vendor Managed Inventory (VMI) monitor in MyFabory, offering insights into historical consumption and our performance. The combination of tailored solutions and actionable insights is genuinely unique.

Our Application Engineers are here to provide solutions and expert advice on fasteners, designs, and applications. In addition to these services, Fabory's experts conduct calculations and tests to ensure secure connections. We collaborate closely with standardisation bodies and technical committees to maintain high technical knowledge and support. This commitment fosters Peace of Mind, allowing you and your team to focus on your core tasks.

Please get in touch with us to explore the possibilities further.

Food_Process.png

Punctele noastre tari

Gama de produse

Fabory este alegerea potrivită pentru toate nevoile dvs. de fixare. Portofoliul nostru de produse conține o gamă largă de elemente de fixare standard și soluții de fixare specifice pentru diverse aplicații precum si C-parts.

Fabory Logic

Fabory Logic va pune la dispozitie o gama completa de servicii lde gestionare a stocurilor printre care RFID, Optical-Eye, Cântare și Merchandiser

Inginerie si controlul calitatii

Fabory este construit pe calitate și fiabilitate. Managementul calității este în centrul operațiunii noastre. Inginerii noștri sunt disponibili pentru a vă sprijini în asigurarea alegerii corecte a elementelor de fixare.

Ne fermez pas cette page. Ce message disparaîtra lorsque la page sera entièrement téléchargée.