text.skipToContent text.skipToNavigation

Uwaga! Od 14 lipca br. następuje aktualizacja kosztów dostawy. Szczegóły w Wiadomościach.

Headassortimenta.png

You no longer have to search for articles yourself

The Fabory range now numbers over 120,000 fasteners and continues to grow. Such an extensive range also requires extensive options when it comes to putting together specific kits. By receiving a kit, your employees on the shop floor do not have to search for separate items. It ensures an even more efficient way of working. You will receive a tailor-made kit and you can be sure that you have the desired items in the right quantities at all times.
 

Kitzakje3.png

Always the right kit

You want processes to run smoothly in the performance of daily activities. Whether you are responsible for the assembly of a specific product or your maintenance of a machine: you do not want to think that one item is missing. Nuts in various designs, blind rivets, threaded rods. Whatever the composition, you need to be able to rely on the right kit for your production assembly.

As a total supplier, Fabory takes care of this for you. We supply special items, standard items and C-parts on a weekly basis in assembled kits. One assembled kit can already consist of a bolt, two washers and a nut. Your own employees work with these kits, or the technicians who take such a kit with them every day. After all, it is often the same products that are assembled for a specific application.

assortiment_icon.png

Small Sets

Four black galvanised screws, four nylon plugs, four washers and a screw bit. Together they come in a small bag. Your technicians or customers always have the right amount of fasteners at hand for the installation of your product.
Plaatje2.png

Module sets

A box containing precise numbers of various sizes of stainless steel hexagon socket screws, lock washers, nuts and plastic covers. All fasteners you need for the assembly of a machine in series production.
Plaatje1.png

Project Kits

Large assembly projects require a comprehensive specification of various fasteners. Large size bolts and nuts in a high strength class, special studs and giant dowel pins. Examples of articles that together form a kit for the construction of a windmill in large volumes.

Efficiency in the workplace

You don't have to do it all yourself. Of course you can put nuts, bolts and washers in a box on your own, but you don't have to. It works a lot more efficiently when fasteners come in composite bags or in pallets stacked on top of each other. With a specific installation, you do not have to wonder whether you have all the necessary mounting materials at hand. Fabory supplies you with the required fasteners as a complete set, in the quantities you need. The kits vary in size: from a bag to a pallet. Whatever the size, the kit is tailored to your daily processes.

Working efficiently prevents mistakes. By preventing errors, you save time and costs. By putting together all the necessary fastening materials in specific kits, Fabory helps you make an efficiency improvement. Together we streamline your processes and lower your Total Cost of Ownership (TCO).

Kittingoverview.png
 
 
"For some customers, the correct delivery of the kit is just as important as the items themselves. After all, processes have to keep running." 
Jos Lavrijsen
Product Category Manager bij Fabory

Customer-Specific

The majority of fasteners from a composite kit come from the standard range. We purchase about twenty percent of the fixing materials from a kit separately. As soon as the articles are in, we will add them. A bolt of M8x30 or M8x40 is in stock at Fabory. Do you just need a bolt of M8x37? Then we add it to the kit. In addition to deviating sizes, the fasteners can also have a deviating surface coating. Still, other customers want all articles in a hot-dip galvanised version. That too is possible. The kits are only assembled when all components are present.

Each kit can be custom-assembled within the frequency you wish. Think of the motor assembly of a windmill, where one kit arrives at its final destination via three pallets. Fabory takes care of everything. This concerns the right items at the right location, in the right numbers, quality management and traceability.

Are you curious about how we can put together kits for you? We are happy to tell you more about it! Do you have questions about the Fabory range? Send an e-mail to our colleagues from Product Category Management.

Did you find this page interesting? There is much more to tell about the Fabory range. Also, view the pages below:

Nasza mocna strona

Dzięki doradztwu, obliczeniom i testom dochodzimy do właściwego projektu i zastosowania konkretnych elementów złącznych. Asortyment 120 000 elementów złącznych w każdej pożądanej wersji, rozmiarze i rodzaju materiału wymaga sprawnego zarządzania zapasami, na którym można polegać. Pomogą Ci w tym inteligentne rozwiązania logistyczne. Fabory Jakość & Inżynieria doradza klientom w zakresie najbezpieczniejszego połączenia. W ten sposób tworzymy spokój ducha. Pracownicy Twojej firmy mogą nadal koncentrować się na podstawowych zadaniach.

Asortyment

Fabory to właściwy wybór dla wszystkich Twoich potrzeb w zakresie elementów złącznych. Nasze portfolio, to szeroki asortyment standardowych elementów złącznych i indywidualnych, specyficznych dla klienta rozwiązań, uzupełniony o części typu C.

Fabory Logic

Fabory zapewnia dostępność elementów złącznych i części typu C. Innowacyjne rozwiązania zapewniają wgląd w zużycie materiałów, redukując całkowity koszt posiadania (TCO). Fabory Logic, to rozwiązania RFID, Optical-Eye, wagowe oraz wsparcie Merchandisera.

Jakość, inżynieria oraz badania i rozwój

Fabory bazuje na jakości i niezawodności. Dopracowane zarządzanie jakością i wyspecjalizowane systemy kontroli są podstawą naszej działalności. Nasi inżynierowie pomogą Ci we właściwym wyborze elementów złącznych dla konkretnego zastosowania.

Nie zamykaj tej strony. Ten komunikat zniknie, gdy strona zostanie w pełni załadowana.