text.skipToContent text.skipToNavigation

Uwaga! Od 14 lipca br. następuje aktualizacja kosztów dostawy. Szczegóły w Wiadomościach.

Innovatie_header.png

Collaborations grow the Fabory range and pave the way for innovation. As a market leader with a decisive position in the market for fastening technology, we include the wishes of our customers in every development. We have been doing this with great pleasure for 75 years. Customers know us as the Masters in Fasteners! Together we come up with new ideas and develop innovative fasteners. Fasteners that help you organise processes more efficiently. Our extensive network of suppliers helps us with the realisation. On this page we explain some examples of innovative fasteners from the Fabory range.

NL.png

Nord-Lock

Nord-Lock offers innovative fasteners like the SUPERBOLT Load-Sensing Tensioner (LST) and the SUPERBOLT Load-Sensing Flexnut (LSF), enriching the Fabory range. Both systems are available from M36 to M100 and measure bias in installations. The data can be monitored remotely or on-site with an accuracy of about 95%. This monitoring method is considered an innovation in industries such as petrochemistry and energy, particularly in the case of large-diameter bolts or nuts requiring pretension. Here are some advantages of LST and LSF:

  • There is no need for construction changes, including geometry and bolt or connection design
  • Accurate monitoring/reading of pretension without adjusting the connection, even remotely
  • Suitable for retrofit/upgrade
  • Robust and reliable, class IP67
  • There are no high costs for labour, extra measuring equipment, and periodic preventive maintenance.

View the full Nord-Lock range

 
 
"Nord-Lock's Load-Sensing Tensioner and Flexnut are two of its most innovative Industry 4.0 products. Both systems' effortless installation, remote monitoring option, and stunning accuracy provide the user Peace of Mind.
Jos Lavrijsen
Product Category Manager bij Fabory

Another example of innovation is our product Lubrinox, which provides lubrication for stainless steel articles. You don't have to apply the lubrication yourself; Fabory does it. You can read more about this application, which is well-suited for use in the food industry, among other things.

The Spiralock nut from Stanley Engineered Fastening is designed for connections that experience heavy vibrations, such as in goods transport, conveyor belts, agriculture, and machine construction.

The unique feature of the Spiralock concept is that the nut has a self-locking internal thread with a 30-degree wedge, eliminating the need for additional locking mechanisms in the connection.

Dorset used Spiralock self-locking nuts because they need heat-resistant lock nuts when working with the Dorset Green Machine in fire-hazard environments. The nuts are easy to disassemble or assemble over time. Dorset, located in Aalten, develops and produces a range of solutions, from RFID electronics to industrial drying installations. When assembling the Dorset Green Machines, the fitters use Spiralock self-locking A4 stainless steel nuts.

Niek ter Horst, the cooperating foreman at Dorset, explained, "We used to use other stainless steel lock nuts for this application. They damaged the bolt's thread and could no longer be dismantled. Jamming of bolts and nuts should be avoided as much as possible. The Spiralock nut offers a particularly good solution for this."

The most unique features of the Spiralock nut include:

  • A self-locking female thread
  • Freewheeling up to the point of preload
  • Even thread load
  • Can be used with standard bolts
  • Reusable, with 100 per cent guaranteed

Fabory supplies the Spiralock nuts in sizes M6 to M16 from stock. The nuts are available as flange nuts in galvanised steel (strength class 10) and stainless steel A4. For more details, view the full Spiralock range.

Spiralock.png

Captive screws and bolts

No one wants to find screws or bolts in their food in the end. At the same time, securing fasteners in panels and doors that open and close regularly is a challenge. The opening and closing must be smooth, yet the screws and bolts must stay in place.

The Fabory range includes captive screws and bolts equipped with a special clip. This innovative solution was developed by a customer who created the idea. With these fasteners, there's no need to adjust the back panel design. Fabory will have the captive fasteners available in stock from mid-2022.

Onverliesbare schroeven en bouten.png

Do you have ideas for expanding the Fabory range, or would you like to discuss fasteners that can help improve your work efficiency? Our Product Category Management colleagues are available to assist you with this. If you found this page interesting, there is more to learn about the Fabory range. You may also want to check out the following pages:

Nasza mocna strona

Dzięki doradztwu, obliczeniom i testom dochodzimy do właściwego projektu i zastosowania konkretnych elementów złącznych. Asortyment 120 000 elementów złącznych w każdej pożądanej wersji, rozmiarze i rodzaju materiału wymaga sprawnego zarządzania zapasami, na którym można polegać. Pomogą Ci w tym inteligentne rozwiązania logistyczne. Fabory Jakość & Inżynieria doradza klientom w zakresie najbezpieczniejszego połączenia. W ten sposób tworzymy spokój ducha. Pracownicy Twojej firmy mogą nadal koncentrować się na podstawowych zadaniach.

Asortyment

Fabory to właściwy wybór dla wszystkich Twoich potrzeb w zakresie elementów złącznych. Nasze portfolio, to szeroki asortyment standardowych elementów złącznych i indywidualnych, specyficznych dla klienta rozwiązań, uzupełniony o części typu C.

Fabory Logic

Fabory zapewnia dostępność elementów złącznych i części typu C. Innowacyjne rozwiązania zapewniają wgląd w zużycie materiałów, redukując całkowity koszt posiadania (TCO). Fabory Logic, to rozwiązania RFID, Optical-Eye, wagowe oraz wsparcie Merchandisera.

Jakość, inżynieria oraz badania i rozwój

Fabory bazuje na jakości i niezawodności. Dopracowane zarządzanie jakością i wyspecjalizowane systemy kontroli są podstawą naszej działalności. Nasi inżynierowie pomogą Ci we właściwym wyborze elementów złącznych dla konkretnego zastosowania.

Nie zamykaj tej strony. Ten komunikat zniknie, gdy strona zostanie w pełni załadowana.