text.skipToContent text.skipToNavigation
Chtěli bychom vás informovat, že v termínu od 21. 12. 2024 do 1. 1. 2025 bude zákaznický servis uzavřen. Vaše objednávky a požadavky budou zpracovány od 2. 1. 2025. Děkujeme za pochopení a přejeme krásné svátky!
Savona_header.png

Favourite products are always at hand in MyFabory.

View prices, view order history, and reorder favourite items. For Dennis Briels, these are the most significant advantages of MyFabory, his online ordering environment at Fabory. He logs in to Fabory.com as a service engineer at Savona in Oisterwijk almost daily.

Savona assists companies with purchasing a wash box installation from the preparation, purchase, and realisation up to and including a complete maintenance program. Their customers are located throughout the Benelux, and Dennis started at the Brabant company in 1996 and kept stocks up to standard for his colleagues in the warehouse.

Various catalogues

Dennis uses various catalogues when ordering fasteners and MRO products. He made it in MyFabory. In addition to bolts, nuts and screws, he added mounting kits and tools as favourites in the catalogues. A few times a month, Dennis completes an order behind his computer. Before he clicks the order button, he walks through the warehouse where his colleagues assemble the wash boxes.

Dennis saves time by placing orders via MyFabory and gains insight into the status of orders, order history and invoices.

All advantages of MyFabory at a glance:

  • Control and overview from one place
  • Insight into order history and invoices
  • Own catalogues with favourite products
  • Personal prices are immediately visible
  • Track orders via Track and Trace
  • Different buyers on the same account
  • Multiple accounts are also possible
  • Easy management of roles and rights

Have you yet to get an account? Create one here

‘I don’t need to know everything by heart.’

Creating catalogues with favourite products in MyFabory is a godsend for Dennis. He immediately sees the products employees reach for on the work floor appear on his screen. In addition to the standard fasteners, these include adjustable wrenches, drills, hose clamps, and mixing nozzles. Dennis also places these in the catalogues; this ensures an efficient way of working. “Just find exactly the version you want. I don’t know all the part numbers by heart. Now you always have every article number at hand. We also work here with a tool called the pop rivet pliers. On Fabory.com, this is called the blind rivet tool.”

Prices and stock level

Dennis is responsible for all orders of fasteners and MRO products required by his colleagues in the warehouse. “In MyFabory, I immediately see whether the desired item is in stock, together with the price. If an item is unavailable, I return to the category type and see what is immediately available.” Savona works with one account. When Dennis is not around, colleagues sometimes log in to the account and add a few articles. “Then they urgently need five hundred bolts in a specific size, for example.

View order history

Dennis is always the one who completes the order. He has been working with MyFabory from day one. “From the moment we no longer had to pass on numbers on pieces of paper, I was convinced. The order history can now always be found. If I have forgotten to place an article in the catalogues, I will still find it there; then I know exactly which special taps are involved.”

Immediately see what is still open.

Dennis’s colleagues can also quickly consult all invoices and packing slips in MyFabory. “My colleagues from Administration check the invoices to see whether the deliveries are correct.” Dennis himself checks his order overviews in MyFabory every week. He can see at a glance what is still open. “If a colleague asks whether specific articles have arrived or are on their way, I can see that immediately. On average, an article arrives at the workplace after one to two days.”

Fixed contact person

Even though Dennis now finalises the orders via MyFabory, his regular contact person at Fabory still visits us now and then. “For example, if a tool is broken, he will send it back to the supplier for me. Switching directly with Fabory and working from my online environment works perfectly for me.”

Always insight into your orders. Also, something for your company?

Do you want to work as quickly and efficiently as Dennis? With MyFabory, you have direct access to your order history and invoices. This ensures overview and control from one place. Experience the benefits of MyFabory and create an account.

Odborníci na spojovací materiál

Díky znalostem výrobků, výpočtům a zkouškám dospějeme ke správnému návrhu a použití konkrétních spojovacích prvků. Náš sortiment 120 000 spojovacích prvků v jakémkoli provedení, velikosti a typu materiálu vyžaduje efektivní řízení zásob, na které se můžete spolehnout. Aplikace RFID je jedním z chytrých řešení, které vám společnost Fabory Logic nabízí. Každé řešení poskytuje cennou podporu pro řízení zásob vaší společnosti. Vytváří tak klid na práci, kdy se zaměstnanci vaší společnosti mohou nadále věnovat svým hlavním úkolům.

Sortiment

Společnost Fabory je tou správnou volbou pro všechny vaše potřeby v oblasti spojovacího materiálu. Naše produktové portfolio obsahuje širokou škálu standardních spojovacích prvků a specifických řešení spojovní pro různé aplikace, doplněných o C-díly.

Fabory Logic

Fabory pomáhá k dostupnosti spojovacího materiálu a C-dílů. Inovativní řídicí panely poskytují přehled o spotřebě a umožňují snižovat TCO (celkové náklady na vlastnictví). Fabory LOGIC vám nabízí řešení jako jsou RFID, Optical, váhy a servis Merchadisera.

Kvalita, zkušenosti a výzkum & vývoj

Fabory si zakládá na kvalitě a spolehlivosti. Základem je propracované řízení kvality a specializované systémy kontroly kvality. Naši inženýři jsou vám k dispozici, aby vám pomohli zajistit správný výběr spojovacího materiálu pro danou aplikaci.

Tuto stránku nezavírejte. Tato zpráva zmizí, jakmile se stránka zcela načte.