text.skipToContent text.skipToNavigation
Fasteners for Semicon & Medical

Always the correct fasteners within reach

Are you involved in the semiconductor and medical industries? If so, you're likely familiar with the high-quality requirements and the strict project-based approach these sectors demand. As a vital part of the production process, it's crucial to ensure that employees do not select the wrong fasteners. Fabory supports you throughout every project stage—from preparation and execution to aftercare (service and repair).

With Fabory Logic's logistics solutions, you can count on optimal fastener availability while keeping your Total Cost of Ownership (TCO) as low as possible.

Fabory assists the semiconductor and medical sectors with the following:

  • The production, construction, and overhaul of CT scan systems, MR imaging systems, and various other medical peripherals
  • The output of lithographic systems used for manufacturing microchips

Medical
© ASML

Clean Room

The cleanliness of your production or assembly processes determines the technical cleanliness required for the fasteners and tools used. In collaboration with our cleaning partners, we ensure that contaminants are removed from products, allowing them to be used in your applications without the risk of contamination. Our cleaning processes target specific types of pollution, including:

  • Residues from the production process, such as burrs and chips
  • Residues from the production environment, including dust, fibres, and sand
  • Stains from process residues, corrosion inhibitors, or fingerprints

The required level of cleanliness will dictate the acceptable amount of the above contaminants and the verification methods needed to confirm compliance. A check with ultraviolet (UV) light may suffice for some applications, while others necessitate a residual gas analysis (RGA).

It is also essential to consider the products' cleanliness requirements and other metallurgical or tribological properties. In some cases, additional measures may be necessary, such as applying an electrolytic polishing and kolsterising (EPK) treatment to ensure product performance in ultra-clean environments.

Are you interested in a cleaning process like this, or do you have different requirements? Please feel free to reach out to us to discuss your possibilities.

Fabory Logic solutions, such as RFID and Weight Scale Cabinets, can be integrated into your cleanroom environment, ensuring that all necessary items are easily accessible.

Elementos de fijación más pedidos

¿Qué elementos de fijación aparecen con más frecuencia en las listas de pedidos de los clientes de este sector? Estos son los diez elementos de fijación siguientes:

Produtos relacionados

En Fabory no sólo somos especialistas en elementos de fijación. Los productos relacionados también forman parte de nuestra oferta. Piense en adhesivos, selladores, lubricantes, herramientas manuales y eléctricas, equipos de seguridad y productos para salas blancas. Ofrecer una gestión inteligente de las piezas C es cada vez más importante. La estrecha colaboración con clientes y proveedores da como resultado una gama de productos, servicios y conocimientos a medida. Los expertos de Fabory le asesoran sobre la facilidad de uso óptima y el rendimiento fiable. No dude en plantearnos sus preguntas sobre soluciones de fijación específicas o sobre el uso de productos relacionados.

Vea nuestra gama completa en Fabory.com

Semicon brands

Por eso el sector Semicon & Medical elige Fabory:

✓ Entrega rápida y flexible de todo tipo de elementos de fijación que cumplan las especificaciones especificadas.

✓Más de 150.000 elementos de fijación diferentes disponibles en stock

✓ En función del uso previsto, le suministramos las fijaciones para salas blancas que necesita en el momento adecuado.

✓ Los elementos de fijación son totalmente trazables gracias al sistema de gestión de calidad ISO9001

✓ Control de calidad en el laboratorio acreditado A2LA de Fabory

✓ Servicios como el inventario gestionado por el proveedor (VMI) in situ e integraciones digitales como MyFabory aumentan su facilidad para realizar pedidos.

Crear tranquilidad

En Fabory, puede elegir entre más de 150.000 elementos de fijación. Están disponibles en cualquier diseño, tamaño y tipo de material. Una gama tan amplia requiere una gestión eficaz de las existencias en la que pueda confiar. A ello contribuyen las soluciones logísticas inteligentes que permiten conocer el consumo. Con el uso tanto de la solución RFID como del armario de pesaje, tendrá acceso a su propio monitor VMI en MyFabory. Esto permite conocer el consumo histórico de las existencias y nuestro rendimiento. La combinación de ofrecer soluciones y proporcionar información es única.

Además de estas soluciones, los expertos de Fabory ofrecen asesoramiento, cálculos y pruebas. Ayudan a realizar conexiones seguras. Esto crea tranquilidad, para que usted y sus empleados puedan seguir centrándose en las tareas principales.

Póngase en contacto con nosotros para hablar de las posibilidades..

Medical

Naše síla

Sortiment

Společnost Fabory je tou správnou volbou pro všechny vaše potřeby v oblasti spojovacího materiálu. Naše produktové portfolio obsahuje širokou škálu standardních spojovacích prvků a specifických řešení spojovní pro různé aplikace, doplněných o C-díly.

Fabory Logic

Fabory pomáhá k dostupnosti spojovacího materiálu a C-dílů. Inovativní řídicí panely poskytují přehled o spotřebě a umožňují snižovat TCO (celkové náklady na vlastnictví). Fabory LOGIC vám nabízí řešení jako jsou RFID, Optical, váhy a servis Merchadisera.

Kvalita, zkušenosti a výzkum & vývoj

Fabory si zakládá na kvalitě a spolehlivosti. Základem je propracované řízení kvality a specializované systémy kontroly kvality. Naši inženýři jsou vám k dispozici, aby vám pomohli zajistit správný výběr spojovacího materiálu pro danou aplikaci.

Do not close this page. This message will disappear, when the page is fully loaded.