text.skipToContent text.skipToNavigation
Header2.png

Fasteners for every industry

The Fabory range continues to grow. With a wide and deep range of fasteners, we provide customers with items from different product categories in many variants. When there is a need for adjustment or expansion, new fasteners are added to the more than 120,000 fasteners that are already in the range.

Keeping assortment relevant: a continuous process

After our start in 1947, a broad customer base arose. We like to hear the stories of our customers: this is how we get to know the challenges they face. These challenges show where further development and expansion of the range are needed. Our customers come from different industries we therefore need to keep updating specific industry knowledge. This translates into our range: industry-specific knowledge enriches the Fabory range of products and keeps it relevant.

An industry-specific approach meets customer needs. These could be customers from the machine-building industry who focus on the food industry. Or customers from the Semiconductor & Medical industry. Other examples of sectors in which we specify the Fabory range are the Truck, Trailer & Coachbuilding, Petrochemistry and the Energy sector.

We highlight two sectors for you:

  • Truck, Trailer & Coachbuilding
  • Machinery for the food industry
Knapen Fasteners for Truck & Trailer Building

Truck, Trailer & Coach building

The Truck, Trailer & Coach building industry has been an crucial industry for Fabory for decades. As a customer in this sector, we now also serve you on the basis of a stock principle.

These are the most frequently ordered fasteners from the Fabory range by customers in this industry:

We have already supplied you as a customer with steel nuts, but we can supply steel nuts with a zinc flake surface coating is a good example of industry-specific work. The need for this product was increasing and because production in the Truck, Trailer & Coach building industry must never stagnate, Fabory supplies 2,000 articles in zinc flake from stock. Where other zinc layers often become too thick, the zinc flake coating has a thin layer thickness with a high corrosion resistance.

Trailer manufacturer

Knapen Trailers from Deurne in Brabant uses 60 unique zinc flake fasteners from Fabory. On the shop floor of the producer of moving floor trailers, employees reach for many thousands of Fabory articles with a zinc flake treatment every week. Johan van Hommelen, a strategic purchaser at Knapen Trailers, explains that the corrosion resistance of the fasteners is an crucial factor for the company. “Our trailers, and therefore also the fastening materials used, are exposed to wind and weather year after year. The influence of the weather on the materials is significant.”

Hundreds of zinc flake fasteners disappear in every trailer: the chassis, the floor frame, the superstructure and various trailer components. The stock management of the zinc flake fasteners remains stable thanks to an RFID solution. “The complete ordering process, including that of the zinc flake fasteners, is taken care of”

Blind Riveting

Blind riveting is a commonly used fastening technique within the Truck, Trailer & Coachbuilding industry. A solution used in almost every bus, truck or trailer. The front to the back and everything in-between the cab, seats, chassis, roof rails, safety structures, floor systems and more.

Depending on the application, a standard blind rivet or blind rivet nut can get the job done. For the more critical applications in this industry, Fabory has structural blind rivets and lockbolts available for you, among other things.

Machinery for the food industry

In the Food Industry industry, customers need to be able to work efficiently with fasteners that comply with strict laws and regulations. The corrosion-resistance of the material makes stainless steel fasteners ideal in this industry, where hygiene is paramount. The stainless steel tap bolt is a commonly used fastener with the hexagon nut.

When using stainless steel fasteners, often the inner and outer threads get stuck together and the fastener can no longer be loosened. Producers in the food industry sector often prevent this cold welding (settling) of stainless steel material by using an assembly paste. Unfortunately, there are drawbacks to this: assembly takes extra time and workpieces and hands must be cleaned after use. We found a solution especially for this industry: a pre-applied lubrication that prevents the screw thread from seizing. The Fabory Lubrinox fasteners are bolts, nuts and screws made of stainless steel with a specially developed coating that provides durable lubrication in the threaded connection. Here are the biggest benefits:

  • It prevents galling of stainless steel bolt connections
  • The Lubrinox coating is approved for use in the food industry
  • The coating has already been applied at Fabory before use. That saves time
  • Lubrinox is also available for nuts
  • The articles retain their stainless steel appearance
  • Lubrinox bolts and screws work great in combination with Loctite
  • Dirty hands from manual lubrication are a thing of the past
  • Less error-prone

FPS-L12 Coating on Fasteners
Counterflow
Stainless steel fasteners go in the Counterflow Cooler Plus

Výrobce chladicích a sušicích zařízení

Konstrukční a výrobní společnost Geelen Counterflow z Haelenu je jednou ze společností, které mohou převzít vedení při testování LUBRINOXU. Spojovací prvky opatřené mazáním zmizely v chladicích a sušicích zařízeních pro potravinářský průmysl. Několik exemplářů těchto chladičů a sušiček je ve společnosti Geelen Counterflow expedováno týdně. Odcházejí do míst po celém světě.

Vzhledem k intenzivnímu používání spojovacích prvků z nerezové oceli hledala společnost nákladově efektivní alternativu k mazání šroubů. René Derckx, technický nákupčí společnosti Geelen Counterflow: "Byli jsme zvědaví, zda řešení navržené společností Fabory splní i naše přání. Hlavním předpokladem bylo, že se závity nezasekávají. Nechceme přece, abychom museli šroub vyřezávat nebo vrtat."

Další nátěr, který zaměstnanci používají na pracovišti, je mnohem silnější. Spojovací materiál LUBRINOX od společnosti Fabory tak silnou vrstvu nepotřebuje. "Silná vrstva znesnadňuje ruční šroubování. Velmi se mastí. Pokud potřebujete použít sílu, přejeďte prsty po šestihranu. To se vám u spojů LUBRINOX nestane. Reakce na dílně jsou při tomto testu pozitivní. "



Odvětví, která podporujeme:

  • Automobilový průmysl, karosářství a výroba přívěsů
  • Elektrická zařízení
  • Energetika (větrná)
  • Nábytek a interiéry
  • Obranný a námořní průmysl, letectví a kosmonautika
  • Ocelářství a těžební průmysl
  • Ocelové konstrukce
  • Petrochemie
  • Polovodičový a zdravotnický průmysl
  • Stavba lodí a jachet
  • Strojírenství
  • Výrobci a montážní firmy
  • Zpracovatelský průmysl

Pokud nemůžete spojovací materiál najít, zajistíme, aby mohl být dodán. Pokud jiný výrobce danou položku nemá nebo pokud se jedná o neexistující položku, navrhneme ji sami nebo ji necháme vyrobit.

 Přečtěte si příběh o hloubce a šíři našeho sortimentu zde. zde.

Naše síla

Pomocí poradenství, výpočtů a zkoušek dospějeme ke správnému návrhu a použití konkrétních spojovacích prvků. Sortiment 120 000 spojovacích prvků ve všech požadovaných provedeních, velikostech a typech materiálů vyžaduje efektivní řízení zásob, na které se můžete spolehnout. S tím vám pomohou chytrá logistická řešení. Fabory Quality & Engineering radí zákazníkům s nejbezpečnějším spojením. Tím vytváříme klid na duši. Zaměstnanci vaší společnosti se mohou nadále soustředit na hlavní úkoly.
 

Sortiment

Společnost Fabory je tou správnou volbou pro všechny vaše potřeby v oblasti spojovacího materiálu. Naše produktové portfolio obsahuje širokou škálu standardních spojovacích prvků a specifických řešení spojovní pro různé aplikace, doplněných o C-díly.

Fabory Logic

Fabory pomáhá k dostupnosti spojovacího materiálu a C-dílů. Inovativní řídicí panely poskytují přehled o spotřebě a umožňují snižovat TCO (celkové náklady na vlastnictví). Fabory LOGIC vám nabízí řešení jako jsou RFID, Optical, váhy a servis Merchadisera.

Kvalita, zkušenosti a výzkum & vývoj

Fabory si zakládá na kvalitě a spolehlivosti. Základem je propracované řízení kvality a specializované systémy kontroly kvality. Naši inženýři jsou vám k dispozici, aby vám pomohli zajistit správný výběr spojovacího materiálu pro danou aplikaci.

Non chiudere questa pagina. Questo messaggio scomparirà quando la pagina sarà completamente caricata.